LOVATO LAB is the R&D laboratory of LOVATO Electric specialised in R&D testing.
The laboratory is born from the need to expand the company’s testing capabilities for the development of new high-performance products, ensuring the highest standards of safety and reliability while reducing time to market. With this laboratory LOVATO Electric joins a very small group of companies able to run power tests at high current values.
The laboratory has a total area of 1700 m2 and has a large technical staff.
The LOVATO Electric laboratory quality system complies with the international EN/ISO/IEC 17025 standard and is accredited by leading national and international bodies such as LOVAG/ACAE and IMQ to run the tests required to obtain product certifications.
The laboratory has been included by IMQ in its monitoring programme as CTF2 for testing products for compliance with established standards.
This enables us to test products for conformity with applicable standards and for CB certification at the same time, thus reducing test times and obtaining third party validation of product performance.

ADVANCED HIGH LEVEL
TESTING EQUIPMENT
LOVATO LAB is equipped with the most advanced machines. They include medium voltage synchronous alternators, a GTEM cell for EMC tests, a synthetic short circuit system rated to 65kA, programmable current generators for temperature and thermal
cutout testing, high precision current generators, isolated high sample rate data loggers and static power breakers. The lab is also equipped with high-speed cameras and thermal chambers for the study of physical
phenomena related to products.
For electrical and mechanical service life testing, it has numerous test benches and a low voltage synchronous alternator for the generation of power up to 1800kVA.
short
circuit
overload
and endurance
glow-wire
test
IP protection
rating
3D x-ray dimensional
controls
taxation planning
Eiusmod tempor incididunt ipsum ut labore dolore magna aliqua. Ut enim minim veniam duisy ipsum sed quis.

SHORT CIRCUIT
Short circuit testing simulates a fault which drastically reduces the impedance of the electrical circuit.
The test part is subjected to a high current and power, and must be able to handle them without risk of injury or damage.
The results of this test enable us to improve the characteristics of the product, whether it is required to break the short circuit or handle it without damage.
taxation planning
Eiusmod tempor incididunt ipsum ut labore dolore magna aliqua. Ut enim minim veniam duisy ipsum sed quis.
OVERLOAD AND ENDURANCE
Overload and Endurance tests subject the product to anomalous operating conditions to test their service life. Depending on the application, a product may be required to handle up to 10 times its rated current and interrupt 8 times that value (overload), as well as execute a high number of operations at its rated current (Endurance).

taxation planning
Eiusmod tempor incididunt ipsum ut labore dolore magna aliqua. Ut enim minim veniam duisy ipsum sed quis.

GLOW-WIRE TEST
The Glow-Wire test is one of the most important tests for verifying the fire resistance of electrical and electronic equipment.
Connections and components can overheat in case of overload or short circuit.
The test verifies the flammability of plastic materials under high thermal stress, their ability to extinguish themselves and their propensity to propagate fire.
taxation planning
Eiusmod tempor incididunt ipsum ut labore dolore magna aliqua. Ut enim minim veniam duisy ipsum sed quis.
IP PROTECTION
RATING
Standards bodies have established a protection rating classification for electrical equipment housings subject to the ingress of foreign bodies.
The second digit in an IP rating refers to the capacity of the housing to prevent the ingress of water in specific installation conditions and at given water flow rates and speeds.

taxation planning
Eiusmod tempor incididunt ipsum ut labore dolore magna aliqua. Ut enim minim veniam duisy ipsum sed quis.

3D X-RAY
DIMENSIONAL CONTROLS
INDUSTRIAL TOMOGRAPHY APPLIED TO METROLOGY AND MATERIALS ANALYSIS
Standards bodies have established a protection rating classification for electrical equipment housings subject to the ingress of foreign bodies.
The second digit in an IP rating refers to the capacity of the housing to prevent the ingress of water in specific installation conditions and at given water flow rates and speeds.
Design, technology, and reliability.
We are an Italian industrial leader that combines the passion of a family business with the solidity of an international company with over 100 years of experience.
We design and manufacture electrical components for low-voltage industrial applications and have always invested in research and development, with strong roots in Italy.
At our headquarters in Bergamo, design, engineering, and innovation come together every day to create reliable, advanced, and tailor-made technological solutions.
LOVATO Electric has been a family-run business for four generations, but with an open, dynamic, and future-oriented entrepreneurial vision. It is precisely this balance between tradition and innovation that has allowed us to grow steadily, building a solid international network: today we are present in over 100 countries, with 14 foreign branches and 90 importers worldwide.
We offer a wide range of products, great flexibility, and a rapid response that makes the difference. Our added value? The high quality of an Italian brand combined with a global presence.