For
89 years, LOVATO Electric has grown and developed in the market of
electromechanical and
electronic
components for electrical equipment.
LOVATO Electric, one of the first companies in
Italy to obtain ISO 9001 certification in
1992, offers over 10,000 product codes
complying with the strictest international standards.
Motor
protection circuit breakers, contactors, push buttons, limit switches,
soft-starters,
relays,
digital multimeters and power factor
regulators are just some of the products totally designed and produced by LOVATO Electric.
LOVATO Electric in Italy together with its 8 foreign Companies and 82 official distributors, is the reference
point for the international distribution of LOVATO Electric products in over
100 Countries.
LOVATO Electric can only develop its activities
by successfully utilising the potential, culture and knowledge of its
collaborators. A ‘TEAM’ that benefits both Customers and
Suppliers.
Company Video
1922
1st Factory
1922
LOVATO
Electric was set up in Bergamo with the
aim of manufacturing air-break and oil-break switches.
1948
Transformation from the production of switches
to that of bus-bar or terminal board contactors.
1960
Start of the production of one-piece
contactors that were to gradually replace the bus-bar or terminal board versions.
1963
New factory
(now central headquarters) in
Gorle (BG) covering an area of 14,000m².
1975
Integration of the "historical"
production of electromechanical components with electronic product lines.
1979
Opening of the first foreign
LOVATO
Electric
factory.
1992
Quality System certification in compliance
with ISO 9001 standards.
1999
Launch of the SM
series, motor
protection circuit breakers with thermal and magnetic trip releases.
2000
Opening of LOVATO Electric in Spain.
Purchase
of the limit switches division business from the Reiter S.r.l. Company.
2001
Opening of LOVATO Electric in USA.
ACAE/LOVAG certification, per European EN 45001 standards, of our
test laboratory.
2002
Obtained the Environment
Management System certification according to ISO 14001 standard
requirements and inauguration of the new R&D facility (3,500m²).
2003
Launch of the K series,
position and safety limit switches.
2004
Launch of Modulo system of
modular components for installation.
2005
Opening of LOVATO
Elctric in Poland.
2006
Launch of Orange system of
motor starting and power applications.
2007
Opening of LOVATO Electric
in Canada.
2009
Launch of
GA series, 16A to 125A
switch disconnectors.
2010
Launch of DMG series, multimeters and power analyzers.
Beginning of the factory expansion work in Gorle (BG).