What do the two values of breaking capacity
Icu and Ics, indicated for motor protection circuit breakers,
represent?
The breaking capacity of a motor protection
circuit breaker is established by tests conducted according to
product standards, IEC/EN 60947-2, and is divided in two
categories: Icu: Rated ultimate
short-circuit breaking capacity Ics: Rated service
short-circuit breaking capacity
The tests include the sequence of operations:
O - t - CO for Icu
O - t - CO - t - CO for Ics, whereas:
O =
a breaking operation in
short-circuit conditions. In this phase, the circuit breaker
will be connected by an external device
t =
time interval between
two successive short-circuit operations
CO =
a making operation followed
by a breaking operation in short-circuit conditions.
After these tests,
the breaker undergoes verifications for dielectric withstand and
overload releases operation. Only for the Ics capacity, testing
also includes over-temperature and operational performance (opening
and closing at rated voltage and current values) verifications.
Specifically speaking, the standard prescribes the breaker must
maintain its performance characteristics after it has tripped
for short-circuit conditions at Ics value while some of these
can be reduced after tripping for short-circuit conditions at
the Icu value .